News

News Feed
May 23, 2013VID-NXTTN Compatible with Reference GTX 780
Koolance has confirmed compatibility with the VID-NXTTN water block and NVIDIA GeForce GTX 780 (original reference layout). A second hardware pack with alternate screws is now being supplied with the block.
Mar 18, 2013Koolance VID-NXTTN (TITAN) Block Now Available!
Koolance's full coverage VID-NXTTN for the NVIDIA GeForce GTX TITAN block is now available. An aluminum back plate is included.
Feb 27, 2013GTX TITAN Water Block Coming Soon!
Koolance will release a full coverage water block for the NVIDIA GeForce GTX TITAN soon. Customers can currently opt-in for an email notification upon arrive. Pictures and pricing will be posted shortly before launch.
Feb 11, 201312V or 24V Speed Controller with Display
The CTR-CD1224 fan and pump controller with display will power 12V or 24V pumps. This includes all current Koolance models: PMP-300, PMP-400, PMP-450, PMP-450S, and PMP-500.
Jan 19, 2013New Quick Disconnects Launched!
Koolance has released a new generation of no-spill quick disconnect couplings. The QD2, QD3, and QD4 series provide easier "push" connection and disconnection by way of an outer locking ring. The new fittings have the same flow performance as earlier no-spill models, but add greater durability and more convenient attachment.
Dec 27, 2012New Years Holiday Closure
Koolance will be closed on Monday, 12/31 and Tuesday, 1/1.
Dec 20, 2012Holiday Closure
Koolance will be closed for the holidays on Monday, 12/24 and Tuesday, 12/25.
Dec 17, 2012Martin Reviews the PMP-500 Pump
The PMP-500 does most things outstandingly well. It has a great price, build quality, g1/4 barb compatibility, built in heat-sink, and about double the power of the PMP-450 all while actually getting smaller in size. The hydraulic performance is nothing short of amazing and can push through pretty much any build out there... King of 12V single pump performance.
Dec 12, 2012PureOC Reviews the CPU-380I
Astonishingly, the Koolance CPU-380 outperforms all of today’s top blocks in both single and dual pump configurations... Koolance’s CPU-380I is an all-around great water block that has a sleek and robust design... Overall there’s a lot to like about the Koolance CPU-380I.
Nov 19, 2012Koolance Closed Nov. 22-23
Koolance will be closed for the Thanksgiving Holiday on November 22nd and 23rd.
Aug 1, 2013New CPU-380 Water Blocks!
The new CPU-380I (Intel sockets) and CPU-380A (AMD sockets) are now available. The Koolance CPU-380 sets a new standard for manufacturing quality and thermal performance. From the microfin cold plate and flow path to the mounting hardware, every aspect of the block has been refined with unprecedented results.

See Stren's review here for performance results:

Highly Recommended - 10/10. The CPU-380 is an excellent block and performs at the very top of the group. It has good flow, and has good manufacturing quality. It feels solid and there is no reason not to give this the gold award in the roundup.

Sep 24, 2012New PMP-500 Pump
The Koolance PMP-500 offers a high flow rate (16L/min, 4.2 gal/min) and static head pressure (7.5m, 24.6ft) at just 12 Volts. It has native G 1/4 BSP threads for fittings and comes with a detachable mounting bracket.
Sep 12, 2012New 12V or 24V Speed Controller
The CTR-SPD1224 speed controller is a single unit which can adjust 12V pumps and fans or step-up voltage and throttle 24V pumps.
Aug 31, 2012Closed for Holiday on Sept. 3
Koolance will be closed for Labor Day on Sept. 3rd. Orders placed after 12PM Pacific on Friday, 8/31, will be shipped on Tuesday, 9/4.
Aug 28, 2012RP-1200 and RP-1005 Rev.2.0 Update
The RP-1200 and RP-1005 have been updated to revision 2.0. Rear electrical connections have been improved, and the safety shutdown feature can now be configured as a normally-open or normally-closed relay. (For computer use, it should be left on normally-open.)
Jul 31, 2012Paypal Standard Available
For end-users with Paypal accounts, the Koolance web store now accepts Paypal Standard for most orders. Alternative payment methods include credit card (via Authorize or Paypal) and bank wire transfer. Bank transfer may be required for some purchases.
Jul 25, 2012Newegg Water Cooling Dos and Don'ts
Newegg has posted a video with Lee from PCJunkieMods.com showing off some nice custom systems with tips on building your own liquid cooled rig:






Jul 18, 2012ASUS Fusion Water Cooling Video
ASUS has posted a how-to video on water cooling the Maximus V Formula using its integrated Fusion Thermo components and the Koolance CPU-370 and Exos EX2-1055 cooling system.






Jul 13, 2012Copper Core 9x120mm Radiator Now Available
Koolance's largest heat exchanger in brass and copper is now available. This includes a steel outer casing with threaded mounting holes on both sides of the radiator. Mounting hardware for 25mm thick fans is included.
Jul 3, 2012Closed Wednesday, July 4th for Holiday
Koolance will be closed for Independence Day on Wednesday, July 4th.
Jun 29, 2012CPU-370 and CPU-370SI for ASUS Fusion Thermo
Koolance CPU-370 and CPU-370SI water blocks have been approved by ASUS for ROG Fusion Thermo cooling.

May 25, 2012Closed Monday, May 28th for Holiday
Koolance will be closed for holiday on Monday, May 28th.
May 21, 2012Full Coverage Block for GTX 690 Now Shipping!
Our VID-NX690 water block for the GTX 690 is now shipping.
May 7, 2012Save $18 on Radeon 7970 Water Blocks!
The Koolance VID-AR797 water block is currently on sale for $18 off.
May 4, 2012Full Coverage Block for the GeForce GTX 690
The Koolance VID-NX690 is currently being developed for the NVIDIA GeForce GTX 690 video card. Availability is expected later this month. Customers can currently opt for notification to receive an email when the first shipment arrives. Pricing and photos will be posted closer to launch.
Apr 17, 2012Koolance Forums Back Online
The Koolance web forums are available again.
Apr 12, 2012Welcome to our New Website
We are pleased to present our new website format! Please excuse any errors you encounter as we continue working on them (any issues can be reported to our Website Dept.).

Several new website features are now available, including USPS shipping (currently limited to orders under 4 pounds), wishlists, product comparisons, and a streamlined RMA process. We expect to add many new additions over the coming weeks!
Apr 1, 2012Koolance VID-NX680 Now Available
Koolance's full coverage block for NVIDIA's GeForce GTX 680 is now shipping.
Mar 21, 2012Koolance VID-NX680 for NVIDIA GTX 680 Coming Soon!
Koolance's new full coverage block for the NVIDIA GeForce GTX 680 is expected soon. Pricing and pictures will be posted shortly before launch.
Feb 27, 2012CPU-370SA and CPU-370SI Water Blocks Now Available!
Koolance has released new lighter weight, lower cost versions of the high performance CPU-370 water block: CPU-370SA (for AMD sockets), and CPU-370SI (for Intel sockets).