Jul 15, 2008TMS-100K Vista 64-bit Drivers Available
64-bit Windows Vista drivers are now available for the Koolance TMS-100K software interface card.
Jul 8, 2008PC5-1300 1.3kW Cooling Systems Released
Koolance now offers quad-120mm fan heat exchangers pre-installed into our chassis. The PC5-1326BK, PC5-1326SL, PC5-1336BK, and PC5-1336SL all include a full-length, 4-fan radiator. Multiple pump options are provided, allowing customers to specify which flow type and control is desired.
The first shipment of Koolance VID-428 water blocks for NVIDIA GeForce GTX 260 and 280 video cards is now available. A rear memory heat sink is included with this block.
Koolance is now shipping the first 1300/1700W water cooled PSU-1300ATX-12N power supplies. If inventory has already sold-out, more will be available by July 8th.
Please be sure to read the PSU compatibility page before purchasing the PSU-1300ATX-12N to be aware of its special mounting requirements.
Please be sure to read the PSU compatibility page before purchasing the PSU-1300ATX-12N to be aware of its special mounting requirements.
Jun 18, 2008Koolance GeForce GTX 280/260 Block Coming Soon!
The estimated arrival date of Koolance's water block for the NVIDIA GeForce GTX 280/260, the VID-428, is July 7th (previously July 2nd). Hit the "Notify" button if you would like to receive an email when they arrive. Pictures and specifications will be posted as soon as they are available.
Jun 17, 2008Virtual Hideout Compares the CPU-340 and CPU-330
The new changes have really helped increase its cooling performance. It easily cooled the CPU by more than 4 degrees over the CPU-330. The cooling performance is on part with that of the DangerDen MC-TDX and D-Tek Fuzion CPU Coolers. The nickel design looks excellent as always and compliments the performance for those serious about their CPU cooling blocks.
By demand, Koolance is now offering a custom manufactured Voltage Regulator Wing for the VID-387 water block. This will allow compatibility with Sapphire (models 11122-03 and 100225) ATI Radeon HD 3870 512MB video cards.
Jun 4, 2008Koolance Customer Gallery!
Have an impressive picture or video of your Koolance build? Or perhaps you are using Koolance products in a unique way? Let us know and we just might post it in the new Customer Gallery.
May 30, 2008International Shipping Costs Decreased
Koolance has significantly reduced shipping rates for all UPS international air methods. This affects orders placed on our website with shipping destinations outside of the United States.
The CPU block performed very well compared to Intel's massive air cooler. The GPU block demonstrated very impressive temperature drops. The GPU block alone is enough to make one want to switch to the Koolance system.
May 23, 2008VID-398GX2 Price Adjustment
Due to even greater demand than anticipated, Koolance has accelerated production of the VID-398GX2 and will be importing by air instead of ocean. Unfortunately, these changes have regrettably increased this item's cost.
Koolance's VID-398GX2 water cooling block for NVIDIA's GeForce 9800 GX2 video card is now available in very limited quantities. We expect these to run out quickly, but greater volume is being produced for arrival over the next 2-3 weeks.
Koolance is now offering its unique brushed & anodized aluminum top radiator/fan shroud for separate purchase. These are available for triple and quad 120mm-fan radiators.
May 13, 2008New Koolance High-Quality Radiator Fans
Koolance has added new dual-ball bearing heat exchanger fans to our assortment. Dual-ball bearing fans are highly recommended for their long-term reliability over sleeve bearing. These now include 80mm, 120mm, 140mm, and 220mm in various airflow ranges.
Apr 28, 20081300/1700W Liquid-Cooled Power Supply Delayed
We have unfortunately been required to delay the PSU-1300ATX-12N power supply launch date until late June. We apologize for this inconvenience. Pricing and preliminary pictures have now been posted. More pictures will be added as they become available.
Koolance's VID-398 water block for NVIDIA 9800 GTX cards is now available!
Apr 23, 20089800 GX2 Block Feature Update
Due to a feature update, the initial availability date for Koolance's VID-398GX2 water block (for NVIDIA 9800 GX2 cards) has been postponed until May 16th.
Mar 27, 2008GeForce 9800 GX2 and GTX Blocks Coming in April
Koolance will provide updates here as our products progress for the new NVIDIA GeForce 9800 GTX (VID-398) and 9800 GX2 (VID-398GX2) video cards. We expect availability in the second half of April.
Initial specifications have been posted for Koolance's upcoming 1300/1700W (continuous) liquid-cooled power supply. Like our previous model, the patented PSU-1300ATX-12N is submerged in a non-conductive cooling fluid for full component heat transfer. However, there are several key differences! [Customers with PSU opt-in notifications have been automatically transferred to this new product.]
Mar 21, 20081000W Exos-2.5 is Now Available
The 1kW cooling capacity, triple 120mm fan Exos-2.5 external systems are now available!
Koolance has released the LIQ-705 liquid coolant for systems with emphasis on high electrical insulation (also called "non-conductive"). See link for details.
Mar 13, 2008Three New Inline Reservoirs with Fill Port
Mar 10, 2008MVR-40 "Universal" VReg Block Now Available
No more purchasing specific VReg blocks for specific motherboards! Koolance now offers a single block, the MVR-40, for mounting various sizes of voltage regulator components. See the MVR-40 product page for details on choosing a heat transfer plate.
Mar 10, 2008CPU-340 Water Block Now Available
The CPU-340 has improved performance over the earlier CPU-330 by optimizing the flow channel and forcing more coolant down through the heat transfer pyramids. Flatness of the bottom contact surface has also been improved. The CPU-340 is made of copper and brass, with anti-corrosive nickel plating.
Mar 10, 2008CHC-122 and CHC-125 Chipset Blocks Now Available
New, improved-performance motherboard chipset water blocks have been released. The CHC-122 is intended for northbridge chipsets, while the swiveling/angled socket CHC-125 allows more flexibility for southbridge chipsets. Both are made solely from copper and brass, with anti-corrosive nickel plating.
Koolance's VID-387X2 Water Block for ATI's Radeon HD 3870 X2 will be available soon (Mar. 12-17). Please click the "Notify" option to receive an automatic email when inventory arrives.
Feb 22, 2008New Koolance Rads and Enclosures/Risers Released
Jan 30, 2008Koolance HD 3870 X2 Availability Update
Koolance's AMD/ATI Radeon HD 3870 X2 Water block should be available in the next 2-3 weeks. Another announcement will be posted here once pictures and an auto-email notification option are available for this product.
Stay Connected