Earlier News - 2009

Please visit the Koolance Homepage for the most recent news. For product reviews, click here.


Dec 31, 2009
The Koolance MB-ASC3F motherboard block for the ASUS Crosshair III Formula is now available!
Dec 24, 2009
Koolance is now offering copper core, high density (30 fins per inch) heat exchangers for 140mm fans. Single, double, and triple fan models are currently available. 140mm rad sizes can provide higher heat dissipation with less noise than 120mm.
Dec 07, 2009
http://www.koolance.com/press/logos/logo_originpc.gif
OriginPC is among the first system builders to offer ATI Radeon HD 5970 video cards with Koolance liquid cooling. Configurable systems are now available at OriginPC.com.
Dec 02, 2009
The Koolance VID-AR597 for AMD Radeon HD 5970 cards is now available.
Nov 18, 2009
The Koolance VID-AR597 cooler is expected soon. This product is designed for the new AMD/ATI Radeon HD 5970. Please click the "Notify" link if you wish to receive a stock notification email.
Nov 10, 2009
With the latest version of 2.1.26, Koolance has opened the TMS-200 source code under the GNU General Public License.
Oct 27, 2009
Koolance now offers reservoir cylinder bodies, tops, and bases for separate purchase. Configure your own liquid tank by choosing which nozzle and pump attachments you need!
Oct 26, 2009
http://www.koolance.com/press/logos/logo_originpc.gif
OriginPC will be incorporating various Koolance products in upcoming systems, including: water blocks, heat exchangers, pumps, and reservoirs. You can be notified of availability by clicking their logo to the left. Early images are available here and here!
Oct 23, 2009
Used in various industries, plate heat exchangers provide highly efficient heat transfer between two liquids without allowing them to mix. Koolance plate heat exchangers are among the most compact and cost effective available.
Oct 23, 2009
The Koolance MB-ASM3F full-coverage block for the P55 based ASUS Maximus III Formula is now available.
Oct 22, 2009
The Koolance VID-AR587 water block (currently in stock) now supports both the Radeon HD 5870 and Radeon HD 5850. Versions with dual support are labeled on the top cover plate.
Oct 09, 2009
The Koolance VID-AR587 water block is now available!
Oct 01, 2009
Radeon HD 5850 Support Coming Soon
Koolance expects a compatible full coverage video block for the Radeon HD 5850 to arrive around October 27th.
Sep 24, 2009
The Koolance VID-AR587 cooler is expected soon. This product is designed for the new AMD/ATI Radeon HD 5870. Please click the "Notify" link if you wish to receive a stock notification email.
Sep 15, 2009
The first shipment has arrived of the new Koolance 1000W PSU-1000ATX-12N Power Supply.
Sep 14, 2009
Trubritar reviews the Koolance five-pump, multi-computer cooling system, the ERM-3K4U5!
Sep 04, 2009
The Koolance CPU-350 takes the honor of having the best performance, and by a noticeable amount. ... the Koolance CPU-350 is king of the i7.
Sep 04, 2009
The Koolance PSU-1000ATX-12N provides 1000W of continuous output in a smaller and lighter profile than the PSU-1300ATX-12N. It is completely flooded in a special non-conductive cooling liquid and fanless!
Sep 02, 2009
Intel Core i5/i7 Socket LGA 1156 CPU Adapters are now available for the CPU-350, CPU-345, and CPU-340.
Aug 18, 2009
Socket LGA 1156 Core i5/i7 Compatibility Update
The CPU-340, CPU-345, and CPU-350 will require a separate bracket for LGA 1156 processor compatibility. Koolance expects to release these new adapters by September 4th, when they will be available for separate purchase.
Jul 22, 2009
New (patent pending) quick disconnects have been added to Koolance's product line. "VL2N" and "VL3N" are no-spill versions of current shut-off QDC nozzles. Be sure not to mix series (VL2, VL3, VL4, VL2N, VL3N) when connecting, as all are physically different from one another.
Jun 25, 2009
The Koolance VID-NX295S for single board GeForce GTX 295 cards is now available.
Jun 25, 2009
The VID-NX285N is now available for revised GTX 275, GTX 285 1GB, and GTX 285 2GB video cards. For previous reference boards, the VID-NX275 and VID-NX285 are also still available.
Jun 15, 2009
The Koolance VID-NX295S cooler is expected this month. This product is designed for the newly updated single-PCB NVIDIA GTX 295. Please click the "Notify" link if you wish to receive a stock notification email.
Jun 12, 2009
Koolance offers the most efficient liquid cooled memory products available. The RAM-33 physically channels liquid along both sides of every DDR3, DDR2, DDR, FB-DIMM, or SD DIMM, providing full coverage to every chip!
Jun 12, 2009
GTX 275, 285 New Video Board Compatibility
For revised GeForce GTX 275 and GTX 285 video cards, Koolance will have a compatible water block available later this month. The VID-NX275 is still available for original reference versions of the GTX 275.
May 18, 2009
Local Pickup Option Now Available
If you are a customer in Washington State, Koolance now has a "Local Pickup" option for orders placed on the website. Please be sure to read the information provided during checkout on allowed pickup times and required identification.
May 07, 2009
The CPU-LN2 is for cooling enthusiasts using liquid nitrogen. It supports a wide range of current processors, including: Intel LGA-1366, LGA-775, AMD AM2, AM2+, AM3, and others.
Apr 29, 2009
Koolance MB-EVX58CF water blocks for EVGA X58 Classified motherboards are expected to arrive later today.
Apr 28, 2009
Koolance has been working to reduce costs on the new copper core heat exchangers and aluminum models, resulting in a significant price drop!
Apr 16, 2009
Koolance's initial shipment of VID-NX275 blocks for NVIDIA's GeForce GTX 275 video cards is now available.
Apr 15, 2009
The Koolance VID-487 has now been updated to include support for ATI's Radeon HD 4890.
Apr 07, 2009
You asked for them-- Koolance now offers copper core heat exchangers in various sizes and nozzle configurations!
Apr 07, 2009
Koolance's VID-NX275 cooler for the new NVIDIA GeForce GTX 275 will be available later this month.
Apr 03, 2009
The Koolance VID-487 is fully compatible with the new ATI Radeon HD 4890. All that is required is a new set of thermal pads, which will be available soon. The VID-487 product description will be updated to include the HD 4890 once these pads are included. (Pads will also be available for separate purchase.)
Mar 19, 2009
The Koolance TMS-200 main board and optional expansion board are now available for purchase.
Mar 11, 2009
Please see our web forum post for news on Koolance's pre-integrated chassis line.
Mar 09, 2009
The latest version of Koolance TMS software/hardware interface products (TMS-200) will be available for purchase soon. New to TMS-200 is the option for expanded monitoring and control with the TMS-EB200 add-on board. Extra screenshots are available here.
Jan 23, 2009
Koolance's initial batch of VID-NX285 (GeForce GTX 285) and VID-NX295 (GeForce GTX 295) water cooling blocks are now available for purchase.
Jan 13, 2009
The ERM-2K3U continues Koolance's "ERM" series of dedicated liquid cooling systems for special thermal applications. It can provide up to 2000W of potential heat dissipation, and is housed in a lightweight aluminum tower or rack-mountable enclosure. Waterfall also included.
Jan 09, 2009
Koolance is currently producing water blocks for the new NVIDIA GeForce GTX 285 (VID-NX285) and GTX 295 (VID-NX295). These models are expected later this month. Pictures and pricing will be posted once available.
Jan 06, 2009
The VID-LN2 is for cooling enthusiasts using liquid nitrogen. It supports a wide range of current video cards, including: Radeon HD 4870, HD 4870 X2, GeForce GTX 280, GTX 260, 9800 GTX, and 9800 GX2.
Jan 06, 2009
Koolance has released two new products for the ASUS Rampage II Extreme Motherboard. Both handle the northbridge and southbridge chipsets (and other nearby components) simultaneously.
Jan 05, 2009
Five new hose colors have been added in 13mm (1/2") ID and 10mm (3/8") ID sizes. Like all Koolance tubing, a special PVC blend make them durable, kink-resistant, and easy to work with. New colors include UV Blue, UV Green, UV Orange, Silver, and Black.