Memory Coolers
Koolance RAM-33
The RAM-33 has no particular limit to the number of consecutive DIMM slots which can be cooled. It has regular perpendicular nozzle sockets, so practically any type of connection can be made using traditional tubing methods. A specific sliding connection nozzle can be used to easily connect blocks.

Installation
To install Koolance RAM cooling blocks, the memory's original heat spreaders or heat sinks (if any) must be removed in order to fit. This provides the highest level of cooling by getting water flow as close to the memory as possible. If your memory sticks have heat spreaders, please verify these can be safely removed before purchasing a Koolance memory water block. Koolance RAM coolers will not fit over existing heat spreaders because they are designed for direct contact with the actual memory chips.

Stay Connected