Feb 22, 2008New Koolance Rads and Enclosures/Risers Released
Jan 30, 2008Koolance HD 3870 X2 Availability Update
Koolance's AMD/ATI Radeon HD 3870 X2 Water block should be available in the next 2-3 weeks. Another announcement will be posted here once pictures and an auto-email notification option are available for this product.
Jan 18, 2008NVIDIA 780i Water Cooling
Our technical support page has been updated with information on water cooling new NVIDIA 780i-based mainboards.
Jan 11, 2008Koolance Announces the New RAM-35 Memory Cooler!
Memory water cooling options from Koolance have been broadened! Available soon, the new RAM-35 (patent-pending) single-slot solution is fully expandable-- liquid cool 1 stick of memory, or 16+ consecutive DIMMs in various flow combinations (series and/or parallel). Also choose from any Koolance G 1/4 threaded nozzles: 1/2" (13mm), 3/8" (10mm), or 1/4" (6mm) internal diameter.
Koolance has released two brand new series of quick disconnect shutoff nozzles. Both are easier to use and offer less flow restriction than the earlier VLV series. The VL2 stresses a low physical profile, while the VL3 offers a higher flow rate.
Jan 7, 2008New Quad and Triple 120mm Fan Radiators
Koolance has released the 1300W HX-1320 Quad 120mm-Fan and the 1000W HX-1020 Triple 120mm-Fan radiators.
Koolance's water cooling block for the NVIDIA GeForce 8800GTS 512MB (65nm) video card is now available.
Koolance's water cooling block for the AMD/ATI Radeon HD 3850 is now available.
Koolance's water cooling block for the AMD/ATI Radeon HD 3870 is now available.
Koolance has released the HD-57 dual hard drive water cooling block for SATA, IDE, SCSI, and SAS drives. The HD-57 includes G 1/4 sockets to allow the use of any available Koolance nozzle diameter, up to 1/2" (13mm) ID.
Dec 17, 2007VID-278 / 8800GT "No Video" Problem
A few customers have contacted Koolance with video problems when using the VID-278 block versus the default heat sink. We have yet to duplicate this problem, but a successful resolution was mentioned when using the Koolance-supplied mounting screws and plastic washers. If true, this would seem to indicate a grounding issue with the default NVIDIA screws and springs. It is therefore recommended to use the Koolance screws and insulating washers (included with the VID-278) to mount the water block.
Dec 17, 2007VID-278 to be Revised for 8800GTS 512MB
The VID-278 water block will be updated in early 2008 for better compatibility with the GeForce 8800GTS 512MB (65nm) card. At this time, Koolance recommends the VID-278 for 8800GT cooling only.
Koolance has updated the PC4 1000W water cooling series with the option to select your nozzle diameter and liquid color. To offer this feature, systems now exclude some necessary components. More details are available at How to Build a Koolance.
Dec 14, 2007New Power Supply Model in Early 2008
Due to additional finalizations, the release of Koolance's newest liquid cooled power supply has been delayed until late January to early February, 2008. The first model available will not be self-cooled or have an external radiator, so it can be connected to an existing water cooling system. Notification for this product can be done here.
The VID-278 Water Block is now available for liquid cooling NVIDIA GeForce 8800GT video cards.
The Koolance CPU-330 cooling block lowered full load CPU temperatures by more than 25°C with essentially the same noise as the stock air cooler. The 8800 GTX video card also ran significantly cooler with the VID-282 cooling block as compared to the stock air cooler. In fact the GPU full load temperatures while being water-cooled with the Koolance waterblock were virtually the same as the idle temperatures on air. Very kool!
Nov 5, 2007Koolance 8800GT Water Block Available Soon
The VID-278 water block is designed for liquid cooling NVIDIA's new GeForce 8800GT video card.
Oct 30, 2007Koolance To Attend SC07 Super Computing Expo
Koolance will be attending SC07 in Reno from November 12-15 at the Reno-Sparks Convention Center. Our booth number is 3232.
Due later this year, Koolance's complete water cooling system for the Sony PS3 will include custom water blocks and mounting hardware, along with an external cooling unit and power adapter.
Aug 22, 2007Koolance To Attend Intel Developer Forum
Koolance will be attending IDF 2007 in San Francisco from September 18-20 at Moscone Center. Our booth number is 637.
Jul 12, 2007Universal Nozzle Body Now Available
Now you can build your own product using any nozzle sizes you want! The Koolance Universal Nozzle Body can make such things as hose splitters, hose adapters, drain valves, and coolant temperature sensors.
Jul 9, 2007New Products RSS Feed
Conveniently stream the most recent products launched by Koolance via RSS!
Jun 28, 2007Koolance Launches the Product Wizard
Not sure which cooling blocks to pick for your hardware? Let us help you!
Jun 22, 2007Radeon HD 2900 XT Cooler Now Available
The Koolance VID-290 GPU+RAM cooling block for ATI Radeon HD 2900 XT cards is now available.
Jun 19, 2007TMS Source Code Available
Source code files for Koolance's Thermal Management Software are now available under the GNU General Public License.
Jun 11, 2007Koolance Radeon HD 2900 XT Cooler Coming Soon!
Available this month, the VID-290 GPU+RAM cooler is designed specifically for ATI Radeon HD 2900 XT cards. It will also work with Koolance connect nozzles in CrossFire configurations.
Jun 7, 2007Exos-2 LX Model Revision
The powerful Exos-2 LX external water cooling system has undergone a revision. Models now (designated "EX2-751") include Koolance shutoff quick-disconnect nozzles and a pump speed controller.
Jun 6, 2007TMS Software Updates: Vista, Open Source
Koolance has verified software compatibility of TMS for use with Windows Vista (the program can be run in "Administrator" mode). Furthermore, Koolance will soon offer the TMS source code online at no charge.
May 11, 2007CPU-330 Revision
Koolance is making a minor revision to the CPU-330 cooler to help avoid component conflicts on some mainboards (such as the eVGA 680i). This change will apply to the CPU-330 coolers available next week. The only alteration is a diagonal beveling of the cold plate.
Stay Connected