Mar 27, 2008GeForce 9800 GX2 and GTX Blocks Coming in April
Koolance will provide updates here as our products progress for the new NVIDIA GeForce 9800 GTX (VID-398) and 9800 GX2 (VID-398GX2) video cards. We expect availability in the second half of April.
Initial specifications have been posted for Koolance's upcoming 1300/1700W (continuous) liquid-cooled power supply. Like our previous model, the patented PSU-1300ATX-12N is submerged in a non-conductive cooling fluid for full component heat transfer. However, there are several key differences! [Customers with PSU opt-in notifications have been automatically transferred to this new product.]
Mar 21, 20081000W Exos-2.5 is Now Available
The 1kW cooling capacity, triple 120mm fan Exos-2.5 external systems are now available!
Koolance has released the LIQ-705 liquid coolant for systems with emphasis on high electrical insulation (also called "non-conductive"). See link for details.
Mar 13, 2008Three New Inline Reservoirs with Fill Port
Mar 10, 2008MVR-40 "Universal" VReg Block Now Available
No more purchasing specific VReg blocks for specific motherboards! Koolance now offers a single block, the MVR-40, for mounting various sizes of voltage regulator components. See the MVR-40 product page for details on choosing a heat transfer plate.
Mar 10, 2008CPU-340 Water Block Now Available
The CPU-340 has improved performance over the earlier CPU-330 by optimizing the flow channel and forcing more coolant down through the heat transfer pyramids. Flatness of the bottom contact surface has also been improved. The CPU-340 is made of copper and brass, with anti-corrosive nickel plating.
Mar 10, 2008CHC-122 and CHC-125 Chipset Blocks Now Available
New, improved-performance motherboard chipset water blocks have been released. The CHC-122 is intended for northbridge chipsets, while the swiveling/angled socket CHC-125 allows more flexibility for southbridge chipsets. Both are made solely from copper and brass, with anti-corrosive nickel plating.
Koolance's VID-387X2 Water Block for ATI's Radeon HD 3870 X2 will be available soon (Mar. 12-17). Please click the "Notify" option to receive an automatic email when inventory arrives.
Feb 22, 2008New Koolance Rads and Enclosures/Risers Released
Jan 30, 2008Koolance HD 3870 X2 Availability Update
Koolance's AMD/ATI Radeon HD 3870 X2 Water block should be available in the next 2-3 weeks. Another announcement will be posted here once pictures and an auto-email notification option are available for this product.
Jan 18, 2008NVIDIA 780i Water Cooling
Our technical support page has been updated with information on water cooling new NVIDIA 780i-based mainboards.
Jan 11, 2008Koolance Announces the New RAM-35 Memory Cooler!
Memory water cooling options from Koolance have been broadened! Available soon, the new RAM-35 (patent-pending) single-slot solution is fully expandable-- liquid cool 1 stick of memory, or 16+ consecutive DIMMs in various flow combinations (series and/or parallel). Also choose from any Koolance G 1/4 threaded nozzles: 1/2" (13mm), 3/8" (10mm), or 1/4" (6mm) internal diameter.
Koolance has released two brand new series of quick disconnect shutoff nozzles. Both are easier to use and offer less flow restriction than the earlier VLV series. The VL2 stresses a low physical profile, while the VL3 offers a higher flow rate.
Jan 7, 2008New Quad and Triple 120mm Fan Radiators
Koolance has released the 1300W HX-1320 Quad 120mm-Fan and the 1000W HX-1020 Triple 120mm-Fan radiators.
Koolance's water cooling block for the NVIDIA GeForce 8800GTS 512MB (65nm) video card is now available.
Koolance's water cooling block for the AMD/ATI Radeon HD 3850 is now available.
Koolance's water cooling block for the AMD/ATI Radeon HD 3870 is now available.
Koolance has released the HD-57 dual hard drive water cooling block for SATA, IDE, SCSI, and SAS drives. The HD-57 includes G 1/4 sockets to allow the use of any available Koolance nozzle diameter, up to 1/2" (13mm) ID.
Dec 17, 2007VID-278 / 8800GT "No Video" Problem
A few customers have contacted Koolance with video problems when using the VID-278 block versus the default heat sink. We have yet to duplicate this problem, but a successful resolution was mentioned when using the Koolance-supplied mounting screws and plastic washers. If true, this would seem to indicate a grounding issue with the default NVIDIA screws and springs. It is therefore recommended to use the Koolance screws and insulating washers (included with the VID-278) to mount the water block.
Dec 17, 2007VID-278 to be Revised for 8800GTS 512MB
The VID-278 water block will be updated in early 2008 for better compatibility with the GeForce 8800GTS 512MB (65nm) card. At this time, Koolance recommends the VID-278 for 8800GT cooling only.
Koolance has updated the PC4 1000W water cooling series with the option to select your nozzle diameter and liquid color. To offer this feature, systems now exclude some necessary components. More details are available at How to Build a Koolance.
Dec 14, 2007New Power Supply Model in Early 2008
Due to additional finalizations, the release of Koolance's newest liquid cooled power supply has been delayed until late January to early February, 2008. The first model available will not be self-cooled or have an external radiator, so it can be connected to an existing water cooling system. Notification for this product can be done here.
The VID-278 Water Block is now available for liquid cooling NVIDIA GeForce 8800GT video cards.
The Koolance CPU-330 cooling block lowered full load CPU temperatures by more than 25°C with essentially the same noise as the stock air cooler. The 8800 GTX video card also ran significantly cooler with the VID-282 cooling block as compared to the stock air cooler. In fact the GPU full load temperatures while being water-cooled with the Koolance waterblock were virtually the same as the idle temperatures on air. Very kool!
Nov 5, 2007Koolance 8800GT Water Block Available Soon
The VID-278 water block is designed for liquid cooling NVIDIA's new GeForce 8800GT video card.
Oct 30, 2007Koolance To Attend SC07 Super Computing Expo
Koolance will be attending SC07 in Reno from November 12-15 at the Reno-Sparks Convention Center. Our booth number is 3232.
Due later this year, Koolance's complete water cooling system for the Sony PS3 will include custom water blocks and mounting hardware, along with an external cooling unit and power adapter.
Aug 22, 2007Koolance To Attend Intel Developer Forum
Koolance will be attending IDF 2007 in San Francisco from September 18-20 at Moscone Center. Our booth number is 637.

Stay Connected