Extra flexible, clear UV-reactive PVC tubing is now available from Koolance in 10mm (3/8in) ID x 16mm (5/8in) OD size.
Dec 5, 2011SSL Certificate Updated
A new website SSL certificate has been installed. Please contact the Koolance web department if any issues remain during login or checkout.
Nov 21, 2011MB-ASR4E Block for ASUS Rampage IV Extreme
The Koolance MB-ASR4E full coverage block for the ASUS Rampage IV Extreme (X79 chipset) is due next week! Customers can opt-in for email notification on stock arrival here. Photos and pricing will be posted as soon as possible.
Nov 14, 2011Koolance Announces Socket LGA 2011 Compatibility
Extra flexible, clear UV-reactive PVC tubing is now available from Koolance in 13mm (1/2in) ID x 19mm (3/4in) OD size.
Oct 6, 2011RP-1200 Now Available
The new 5.25" bay reservoir and pump combo includes Koolance's latest VFD dot matrix display, providing options like a dynamic fan ramp and flow meter feedback.
ERM-3K3U, EX2-1055, EX2-755, and EXT-440 cooling systems are now CE certified. Certificate copies are available here.
A problem has been found with some VL3N and VL4N quick disconnects which can prevent the male or female sides from fully sealing when separated (disconnected). Further details have been posted here. For customers who have encountered this problem, please submit an RMA request to get them exchanged.
The CTR-CD12 is a pump and fan speed controller and temperature monitoring unit in a 5.25" drive bay profile. This unit incorporates all-new Koolance electronics, with a 2-line VFD dot matrix display for deeper user control and feedback.
For 12VDC pumps, the new dual speed controller fits into a single 5.25" bay. It can adjust pumps between 7.5-12.7V, providing a small performance boost to Koolance PMP-400 above 12V.
Aug 21, 2011Green Spring Wrap Color Change
The color of Koolance green tubing spring wrap has been altered by request. It is now a more vivid green color.
Koolance has found and immediately fixed a website vulnerability that could have allowed an attacker to access customer account information. Credit card numbers are not stored by the Koolance website and would not be accessible. Customers are currently being notified by email. As a precaution, all website account passwords have been changed and will need to be reset before logging in again. Please click here for details.
Jun 20, 2011New Phone/Fax Numbers
Koolance USA has a new phone number (253-249-7669) and fax number (253-249-7453). Earlier numbers will be discontinued in the near future.
Jun 19, 2011Save $20 on Radeon HD 6990 Blocks
For a limited time, VID-AR699 (for Radeon HD 6990) full coverage blocks are $20 off the retail price.
If you don't have room for a dual 5.25" reservoir unit, Koolance now offers a single bay version, the RP-401X2!
Jun 1, 2011Koolance Swivel/Lock Barbs Available
Jun 1, 2011RP-402X2 & RP-452X2 Bleed Pipe Kit
Koolance RP-402X2 and RP-452X2 dual bay/reservoir products now include a bleed pipe for installation in the upper reservoir. This eases air filtration if using the right-side tank inlet/outlet. Customers who have already purchased a dual reservoir can request the bleed pipe for free (this offer is good through August). Please click here for details.
May 31, 2011ERM-3K3U Cooling Systems Coming Soon
ERM-3K3U will be Koolance's most powerful system available, with 9x120mm high-flow fans and a 24V PMP-450S pump. For comparison, it provides greater thermal performance at 20% fan speed than previous ERM-2K3U models at 100%. Aluminum or copper core models are offered, both featuring new electronics and a VFD dot matrix display.
Apr 25, 2011Black Nozzles and Fittings Now Available
The first black Koolance nozzles and fittings are now available. More models are on the way!
Apr 3, 2011VID-NX590 Block for GTX 590 now available
The Koolance VID-NX590 is now available!
Mar 31, 2011EXT-440CU External Cooling System Now Available
Koolance's latest EXT-440CU takes the place of earlier Exos-LT compact cooling units. It features a higher speed (swappable) fan, copper core radiator, and a new industrial-oriented format.
Mar 24, 2011VID-NX590 for NVIDIA GeForce GTX 590 Coming Soon
The Koolance VID-NX590 full coverage block for the dual-GPU GTX 590 video card is coming soon! Email notifications can currently be made. Photos and pricing will be posted once available.
Mar 23, 2011VID-AR699 Block Now Available
The Koolance VID-AR699 for AMD's Radeon HD 6990 cards is now available. Another shipment is arriving early next week.
Mar 15, 2011Radeon HD 6990 Block ETA Now 3/25
A production delay has pushed expected availability of the VID-AR699 water block to March 25th.
Mar 7, 2011Radeon HD 6990 Block Coming Soon!
Connection fittings for running serial pumps on the RP-402X2 or RP-452X2 dual reservoir units are now available. Stock won't last long, but another shipment is scheduled for next Monday.
Feb 23, 2011CPU-370 Now Available
Following in the popular CPU-360 style, the CPU-370 contains improvements to the internal core, unlocking performance beyond all previous Koolance blocks!
Feb 17, 2011Save $40 on GTX 480 (Rev.1.1) Video Blocks
Koolance's full coverage block for GeForce GTX 480 cards (VID-NX480) is on sale for $40 off retail price! Revision 1.1 has improved heat transfer performance over the original model.
Feb 1, 2011Powerful 120mm Koolance Fans Now Available
For customers looking solely for best cooling performance, Koolance has started carrying very high RPM/CFM fans beginning with 120x38mm model FAN-12038HBK-184. This is a 2-amp, 4000RPM, 184CFM, high pressure and high dBA fan. Be sure to use it with a fan grill for safety, and make sure your fan controller can support the amperage!

Stay Connected