Jul 12, 2007Universal Nozzle Body Now Available
Now you can build your own product using any nozzle sizes you want! The Koolance Universal Nozzle Body can make such things as hose splitters, hose adapters, drain valves, and coolant temperature sensors.
Jul 9, 2007New Products RSS Feed
Conveniently stream the most recent products launched by Koolance via RSS!
Jun 28, 2007Koolance Launches the Product Wizard
Not sure which cooling blocks to pick for your hardware? Let us help you!
Jun 22, 2007Radeon HD 2900 XT Cooler Now Available
The Koolance VID-290 GPU+RAM cooling block for ATI Radeon HD 2900 XT cards is now available.
Jun 19, 2007TMS Source Code Available
Source code files for Koolance's Thermal Management Software are now available under the GNU General Public License.
Jun 11, 2007Koolance Radeon HD 2900 XT Cooler Coming Soon!
Available this month, the VID-290 GPU+RAM cooler is designed specifically for ATI Radeon HD 2900 XT cards. It will also work with Koolance connect nozzles in CrossFire configurations.
Jun 7, 2007Exos-2 LX Model Revision
The powerful Exos-2 LX external water cooling system has undergone a revision. Models now (designated "EX2-751") include Koolance shutoff quick-disconnect nozzles and a pump speed controller.
Jun 6, 2007TMS Software Updates: Vista, Open Source
Koolance has verified software compatibility of TMS for use with Windows Vista (the program can be run in "Administrator" mode). Furthermore, Koolance will soon offer the TMS source code online at no charge.
May 11, 2007CPU-330 Revision
Koolance is making a minor revision to the CPU-330 cooler to help avoid component conflicts on some mainboards (such as the eVGA 680i). This change will apply to the CPU-330 coolers available next week. The only alteration is a diagonal beveling of the cold plate.
May 11, 2007TMS Vista Drivers Due Soon
Vista-compatible software for the Koolance TMS interface card is expected later this month. We are finalizing drivers now.
Koolance's revolutionary 1200W power supply has obtained NVIDIA SLI⢠certification at the highest level (dual GeForce 8800GTX cards). Allow the world's first truly submerged liquid cooled power supply to handle your most demanding gaming setup.
Tom's Hardware has published an introduction to water cooling that features a good range of Koolance systems and cooling blocks. If you are new to water cooling, this could be a great start!
Mar 12, 2007Motherboard Northbridge Cooler in 10mm (3/8")
The CHC-120-V10 motherboard block is now available with 10mm (3/8") hose barbs!
Mar 8, 2007ASUS Voltage Regulator Cooler in 10mm (3/8")
The 10mm (3/8") VR-AS40-V10 voltage regulator liquid cooler for ASUS motherboards is now available.
Mar 8, 2007Customizable Cooling Kit
Choose exactly which products you wish to bundle together with the Koolance KIT-500. The base kit includes an HX-360 heat exchanger, LED 120mm fan, CPU-330 (with nozzles), liquid coolant, and tubing. Simply choose your pump!
Feb 27, 2007RP-950 5.25" Reservoir & Pump
The RP-950 is a lower priced 5.25" bay reservoir with Koolance's PMP-400 pump. It is similar to the RP-1000, but lacks the LED display or pump control circuitry.
Feb 26, 20071200W Power Supply Availability - End of March
Availability of the PSU-1200ATX-12S has been rescheduled for the end of March. Arrival of all other products are still anticipated this week.
Feb 1, 2007Huge Price Drop!
Koolance has greatly reduced prices on most major products. Save up to $100 on Systems and Exos, up to $25 on Cooling Blocks, and benefit from discounts on many other Koolance accessories!
Jan 24, 2007Liquid Cooled 1200W (Continuous) Power Supply
Available next month, the Koolance 1200W (1400W peak) liquid-cooled power supply achieves greater than 80% efficiency by operating in a completely submerged state. It is also self-cooled, and therefore does not require any additional cooling system.
Jan 19, 2007Announcing the New Koolance CPU-330 Cooler
Now available, the rugged new Koolance CPU-330 provides ultra low temperatures in single or multi-core configurations. The CPU-330 is available with any Koolance G1/4 nozzle type: 1/4", 3/8", or 1/2".
Koolance brings high quality cooling to the fastest gaming cards available. The VID-282-V10 (8800GTX) and VID-280-V10 (8800GTS) include standard G1/4 threaded nozzles for 1/4", 3/8", or 1/2" compatibility. Koolance Connect Nozzles bypass sandwiched cards for easy SLI setup.
Jan 19, 2007New CHC-120 Motherboard Cooler
Put heatpipes to shame. The CHC-120-V06 is designed for motherboard northbridge or southbridge chipsets, including those below PCI-Express cards. A newly designed cooler and bracket allows one cooler to fit almost all types of mainboards.
Jan 19, 2007Koolance G1/4 Nozzles
By popular demand, most replaceable Koolance nozzles are now also available in standard G1/4 threading for new products. The new nozzles are gun metal in color. (Koolance's metric-threaded nozzles are silver/chrome.)
Jan 17, 2007Koolance Quad Super Splitter
Going from 1/2" (13mm) or 3/8" (10mm) to 1/4" (6mm) ID has never been easier. Now choose from a full array of up to 4 outlet/inlets. Larger nozzles are included and come in standard G-1/4 threading.
Jan 17, 2007Voltage Regulator Cooler for ASUS Mainboards
The VR-AS40-V06 is designed for VReg circuits on ASUS motherboards of standard spacing. Many new boards can utilize two of these, and in addition to northbridge cooling, eliminates the need for extensive (and less efficient) heatpipes without airflow available.
Nov 29, 20068800GTX/GTS GPU+RAM Cooler Coming
The Koolance "VID" series coolers for the 8800GTX/GTS should be available in January. Another announcement will be made at that time.
Nov 7, 2006HardOCP PC4-1020BK 1kW Series Review
With the ability to dial in the exact performance to noise ratio that suits your needs it would be hard not to find a Koolance PC4 configuration that works well for you. The PC4 series from Koolance is a solidly designed unit that delivers exactly what it promises and possible a bit more.
Oct 23, 2006Exos-2 Sale!
Koolance is celebrating 4 years since the first Exos system was launched. Now through the end of October, Exos-2 and Exos-2+ from Koolance.com are on sale.
Oct 23, 2006EHX-1050 Review at Virtual-Hideout.net
It looks great in just about any installed configuration conceived for every possible use. The EHX should easily please the most avid user demanding results from their kit.
Oct 13, 2006INX3-1050 1kW Combo Kit Available
Combining an external triple 120mm radiator (EHX-1050) with a 5.25" bay reservoir and pump (RP-1000), the INX3-1050 includes everything needed to add 1000W of potential liquid cooling to a 3rd-party chassis. No cutting or drilling is required!

Stay Connected