Liquid Cooling Solutions
Koolance is an ISO 9001 & ISO 14001 manufacturer specializing in custom liquid cooling solutions. We offer tailored engineering and custom product development to meet your specific requirements. We also provide cold plates, sub-assemblies, heat exchangers, chillers, liquid-air cooling systems, pumps, quick connect fittings, and other components involved in ambient and sub-ambient water cooling systems.
iso badge 9001 iso badge 14001
Nov 4, 2025Visit Koolance at SC25 Expo
Koolance will be exhibiting at the SC25 High Performance Computing Expo from Nov. 18-20th. Come visit us at Booth #6432 in St. Louis, MO!
Aug 15, 2025ALX-3000 Coming Soon
A new 3kW ambient liquid cooling system will be available soon. ALX-3000 fills the cooling capacity gap between Koolance's ALX-2000 and larger ALR-4600 systems. Unlike existing ALX systems, ALX-3000 is not modular (it has fixed radiators), and accepts 110~220V AC power instead of 12V DC.
Aug 11, 20252kW Liquid Chiller Now Available
Koolance has released its highest capacity refrigerant chiller to date: VLX-2000-110V. It is rated to 2000W with a 0° liquid-ambient temperature delta (@25°C ambient).
Previous news posts >>