Dec 27, 2012New Years Holiday Closure
Koolance will be closed on Monday, 12/31 and Tuesday, 1/1.
Dec 20, 2012Holiday Closure
Koolance will be closed for the holidays on Monday, 12/24 and Tuesday, 12/25.
Dec 17, 2012Martin Reviews the PMP-500 Pump
The PMP-500 does most things outstandingly well. It has a great price, build quality, g1/4 barb compatibility, built in heat-sink, and about double the power of the PMP-450 all while actually getting smaller in size. The hydraulic performance is nothing short of amazing and can push through pretty much any build out there... King of 12V single pump performance.
Dec 12, 2012PureOC Reviews the CPU-380I
Astonishingly, the Koolance CPU-380 outperforms all of today’s top blocks in both single and dual pump configurations... Koolance’s CPU-380I is an all-around great water block that has a sleek and robust design... Overall there’s a lot to like about the Koolance CPU-380I.
Nov 19, 2012Koolance Closed Nov. 22-23
Koolance will be closed for the Thanksgiving Holiday on November 22nd and 23rd.
Aug 1, 2013New CPU-380 Water Blocks!
The new CPU-380I (Intel sockets) and CPU-380A (AMD sockets) are now available. The Koolance CPU-380 sets a new standard for manufacturing quality and thermal performance. From the microfin cold plate and flow path to the mounting hardware, every aspect of the block has been refined with unprecedented results.
See Stren's review here for performance results:
See Stren's review here for performance results:
Highly Recommended - 10/10. The CPU-380 is an excellent block and performs at the very top of the group. It has good flow, and has good manufacturing quality. It feels solid and there is no reason not to give this the gold award in the roundup.
Sep 24, 2012New PMP-500 Pump
The Koolance PMP-500 offers a high flow rate (16L/min, 4.2 gal/min) and static head pressure (7.5m, 24.6ft) at just 12 Volts. It has native G 1/4 BSP threads for fittings and comes with a detachable mounting bracket.
Sep 12, 2012New 12V or 24V Speed Controller
The CTR-SPD1224 speed controller is a single unit which can adjust 12V pumps and fans or step-up voltage and throttle 24V pumps.
Aug 31, 2012Closed for Holiday on Sept. 3
Koolance will be closed for Labor Day on Sept. 3rd. Orders placed after 12PM Pacific on Friday, 8/31, will be shipped on Tuesday, 9/4.
Aug 28, 2012RP-1200 and RP-1005 Rev.2.0 Update
The RP-1200 and RP-1005 have been updated to revision 2.0. Rear electrical connections have been improved, and the safety shutdown feature can now be configured as a normally-open or normally-closed relay. (For computer use, it should be left on normally-open.)
Jul 31, 2012Paypal Standard Available
For end-users with Paypal accounts, the Koolance web store now accepts Paypal Standard for most orders. Alternative payment methods include credit card (via Authorize or Paypal) and bank wire transfer. Bank transfer may be required for some purchases.
Jul 25, 2012Newegg Water Cooling Dos and Don'ts
Newegg has posted a video with Lee from PCJunkieMods.com showing off some nice custom systems with tips on building your own liquid cooled rig:
Jul 18, 2012ASUS Fusion Water Cooling Video
Jul 13, 2012Copper Core 9x120mm Radiator Now Available
Koolance's largest heat exchanger in brass and copper is now available. This includes a steel outer casing with threaded mounting holes on both sides of the radiator. Mounting hardware for 25mm thick fans is included.
Jul 3, 2012Closed Wednesday, July 4th for Holiday
Koolance will be closed for Independence Day on Wednesday, July 4th.
Jun 29, 2012CPU-370 and CPU-370SI for ASUS Fusion Thermo
May 25, 2012Closed Monday, May 28th for Holiday
Koolance will be closed for holiday on Monday, May 28th.
May 21, 2012Full Coverage Block for GTX 690 Now Shipping!
Our VID-NX690 water block for the GTX 690 is now shipping.
May 7, 2012Save $18 on Radeon 7970 Water Blocks!
The Koolance VID-AR797 water block is currently on sale for $18 off.
May 4, 2012Full Coverage Block for the GeForce GTX 690
The Koolance VID-NX690 is currently being developed for the NVIDIA GeForce GTX 690 video card. Availability is expected later this month. Customers can currently opt for notification to receive an email when the first shipment arrives. Pricing and photos will be posted closer to launch.
Apr 17, 2012Koolance Forums Back Online
The Koolance web forums are available again.
Apr 12, 2012Welcome to our New Website
We are pleased to present our new website format! Please excuse any errors you encounter as we continue working on them (any issues can be reported to our Website Dept.).
Several new website features are now available, including USPS shipping (currently limited to orders under 4 pounds), wishlists, product comparisons, and a streamlined RMA process. We expect to add many new additions over the coming weeks!
Several new website features are now available, including USPS shipping (currently limited to orders under 4 pounds), wishlists, product comparisons, and a streamlined RMA process. We expect to add many new additions over the coming weeks!
Apr 1, 2012Koolance VID-NX680 Now Available
Koolance's full coverage block for NVIDIA's GeForce GTX 680 is now shipping.
Koolance's new full coverage block for the NVIDIA GeForce GTX 680 is expected soon. Pricing and pictures will be posted shortly before launch.
Apr 9, 2012RP Pump+Reservoir Units Now CE Certified
Koolance models RP-985, RP-1005, and RP-1200 products are now CE certified.
Jan 20, 2012Weather Conditions May Delay UPS Shipments
Due to severe winter weather in the Pacific Northwest, some shipments might be delayed while in transit. Weather is expected to improve this weekend.
Jan 8, 2012VID-AR797 for Radeon HD 7970 Coming Soon
The Koolance full coverage VID-AR797 for the Radeon HD 7970 video card is expected next week. Currently, customers can opt in for an email notification once stock arrives. Pricing should be posted shortly.
Dec 19, 2011MB-ASSTX79 Block for ASUS Sabertooth X79
The Koolance MB-ASSTX79 full coverage block for the ASUS Sabertooth X79 is now available.
Dec 18, 2011New Koolance Swiveling Fittings
Multi-segmented swiveling fittings are now available from Koolance in 30, 60, and 90 degrees.

Stay Connected