Mar 16, 2017New Modular ALX Cooling Systems Launched
Koolance's ALX series are powerful liquid cooling systems with expandable thermal capacities and software logging. ALX systems have up to twice the thermal capacity of previous Koolance ambient liquid cooling systems for the same heat exchanger size. As modular products, the radiator and pump units can be individually upgraded if requirements later change.
Feb 28, 2017CPU-390 Gets Support for AMD Socket AM4
Koolance CPU-390A and CPU-390CA water blocks now include support for AMD's socket AM4 (Ryzen, etc.). For existing owners of CPU-390, a separate upgrade kit is available to add compatibility.
Jan 11, 2017MD&M West Medical Expo Feb. 7-9
Aug 17, 2016Acrylic Top GTX 1070/1080
Koolance has released an acrylic-top version of its GeForce GTX 1070/1080 full-coverage video block.
Aug 18, 2016CPU-390 Reviewed at Extreme Rigs
Jun 24, 2016VID-NX1080 Now Available
The Koolance GTX 1080/1070 full coverage block and optional back plate are now available for purchase.
Jun 21, 2016CPU-390 Now Available!
Koolance has released its next generation of CPU water blocks with the smallest microfins yet: 0.17mm. Versions are available with acrylic and copper tops.
Jun 17, 2016GTX 1080 and 1070 Video Block Coming Soon
A full coverage video water block for NVIDIA's GTX 1080 and GTX 1070 is in production. Customers can currently opt-in to receive an email notification when stock arrives for the VID-NX1080. Photos and pricing will be posted in June.
Jan 14, 2016The Witcher Mod
Famed modders Jon (PennyWise) Hansz and Ron Lee Christianson are working on a new Witcher-themed PC with Koolance liquid cooling. Check out their build log here!
Nov 18, 2015Koolance Rigid Tube Fittings
Koolance now offers straight and elbow fittings for acrylic & PETG tubing. All models have triple internal o-rings to improve sealing reliability.
Nov 13, 2015QD1H Quick Disconnects Available
Koolance has launched a new QD1H no-spill quick disconnect series for 1/8 inch (3mm) ID tubing.
Aug 5, 2015Intel Skylake CPU Support
The Koolance CPU-380I is expected to remain compatible with Intel's new Skylake processor. Skylake's socket LGA1151 uses the same cooler mounting pattern as LGA1150.
Jun 3, 2015GeForce GTX 980 Ti Compatibility
Koolance has confirmed the VID-NXTTNX water block and optional back plate are compatible with the new NVIDIA GeForce GTX 980 Ti graphics card.
Apr 15, 2015Titan X Water Block and Back Plate Now Available
Koolance's water blocks and back plates for Titan X are now shipping.
Mar 26, 2015VID-NXTTNX for Titan X Video Cards Coming Soon
Koolance's water block for the NVIDIA GeForce GTX Titan X will be available soon. Photos and pricing will be updated shortly before launch. Customers can currently opt-in for an email notification upon stock arrival.
Mar 11, 2015Xtreme Rigs Reviews the Koolance VID-NX980
Koolance's full coverage block for the NVIDIA GTX 980 was reviewed by Stren:
A very good performance... Honestly the best quality block I’ve ever seen from Koolance.
Xtreme Rigs reviews Koolance's popular and reliable RP-452X2 single/dual pump reservoir:

This is the best dual D5 pump/reservoir combo that we’ve ever seen. The quality and flexibility are amazing... If you need something like this then this is the best choice.

Jan 20, 2015Koolance Releases Compact Chiller EXC-450
Koolance's EXC-450 is an extremely compact (6in x 8in x 21in, or 152mm x 203mm x 533mm) portable recirculating liquid chiller rated at 450W, or 1535 BTU/hr @25°C liquid & ambient. Power input is 24VDC, for which Koolance will soon be offering a separate AC adapter kit.
Jan 9, 2015GPU-220 Revision 2
The GPU-220 water block has been updated with new mounting hardware, supporting higher contact pressure and improving heat transfer.
Dec 8, 2014December Stock Delays
Several inbound shipments have been delayed by the U.S. Pacific Coast port labor slow-down. Estimated arrival dates for out-of-stock products are being adjusted on a daily basis as new information arrives. We apologize for the inconvenience.
Jan 5, 2015Holiday Deals!
For a limited time, a select list of Koolance products are on sale for the holiday season.
Dec 9, 2014Tweak.dk Reviews a Koolance Kit
Tweak.de has reviewed an easy, low-cost kit from Koolance featuring the CPU-380I, PMP-300 pump and reservoir, and HX-CU420V radiator (translated):

The performance was better than expected, and this little cooler fought a good fight to keep my 5820K cool under pressure... The price is in my view absolutely fair, because you really do get what you pay for. Quality across the board. Koolance has proven their worth, and they have done it with style. Therefore, I can not do anything but give the system here today 9.5 + one Editor's Choice Award.
The HD-70 is a double-sided water block for cooling one or two 2.5-inch (SSD and notebook) size hard drives.
Oct 22, 2014Proclockers Reviews INS-FM18D Flow Meter
The Koolance INS-FM18D flow meter with display has been reviewed by Proclockers:
The Koolance INS-FM18D Coolant Flow Meter with Display is [a] simple and effective tool... It is also small enough to fit just about anywhere... We will be adding it to our tool set for future water cooling testing.
Oct 10, 2014VID-NX980 Does Not Include Back Plate
A typo on the item description for VID-NX980 has now been fixed. This water block does NOT include a back plate. It's designed to use the stock back plate (when included) with the GTX 980 video card. The installation manual for this product can be downloaded under the "Files" tab here.
Oct 9, 2014VID-NX980 Water Blocks Now Available
Koolance's blocks for the GTX 980 are now in stock.
Sep 22, 2014GTX 980 Water Block Coming Soon
Koolance's VID-NX980 for the NVIDIA GTX 980 video card will be available soon. Customers can currently opt-in for a notification via email when stock arrives.
Sep 16, 2014Haswell-E / X99 Compatibility
Koolance confirms compatibility with the CPU-380I and socket 2011-v3 used for Haswell-E and the X99 chipset.
Sep 4, 2014Koolance Launches NPT Quick Disconnects
Tapered thread NPT quick connect couplings have been added to Koolance's QD3 series. QD2 and QD4 will also be getting NPT threaded models.
Aug 8, 2014Radeon 295X2 Water Blocks on Sale!
Koolance's VID-AR295X2 water block is currently on sale for $50 off retail.


Stay Connected