Nov 4, 2025Visit Koolance at SC25 Expo
Koolance will be exhibiting at the SC25 High Performance Computing Expo from Nov. 18-20th. Come visit us at Booth #6432 in St. Louis, MO!
Nov 4, 2025ALX-3000 Coming Soon
A new 3kW ambient liquid cooling system will be available soon. ALX-3000 fills the cooling capacity gap between Koolance's ALX-2000 and larger ALR-4600 systems. Unlike existing ALX systems, ALX-3000 is not modular (it has fixed radiators), and accepts 110~220V AC power instead of 12V DC.
Aug 11, 20252kW Liquid Chiller Now Available
Koolance has released its highest capacity refrigerant chiller to date: VLX-2000-110V. It is rated to 2000W with a 0° liquid-ambient temperature delta (@25°C ambient).
Jul 24, 2025Shipping Origin for Web Orders
Customers now have the option to ship from either Koolance U.S. or Koolance Korea when ordering through the website, depending on availability. Inventory and pricing are shown for both locations on the product pages. Please be aware that import duties may be required if your shipment is dispatched from a different country than the destination (which must be paid to the carrier before delivery).
Jul 2, 2025ALR-4600 Now Available!
Aug 11, 2025VLR-600 Rack Mountable Chiller
The VLR-600 refrigerant liquid chiller is now available! This cooling system can be mounted to a 19-inch equipment rack and is 3U in height. Refilling and draining are made easier with front-facing quick disconnects and support for sliding rack rails (rails not included).
Apr 26, 2024New Flow Meter & Temperature Display
Now available is the DCB-FMTP01 display for Koolance flow meters and thermistor temperature sensors. It is compatible with all current flow meter models, including the hall effect INS-FM17H. The display has a configurable audio alarm, and an adjustable flow rate pulse factor for potential support of 3rd-party flow meters.
Mar 21, 2024TLH-300 Thermoelectric Chiller Available
For cooling and heating applications demanding high temperature precision, Koolance has released the TLH-300 TEC chiller. With a temperature accuracy of +/-0.1ºC, it is rated for 300W of cooling (with a 0ºC liquid-ambient delta), and includes heating capabilities.
Aug 1, 2023INS-FM17H Hall Effect Flow Meter
Koolance has released its first flow meter using a hall effect sensor for 3rd-party applications, model INS-FM17H.
Mar 28, 2023New Copper Core 17FPI Radiators
Koolance has released new copper and brass radiators with a fin density of 17 fins per inch. These can be ideal for quieter fan operation at lower airflow ranges. The radiators have dual inlet and outlet ports, offering more flexibility with tubing management or for adding temperature sensors.
The QDT series is Koolance's 6th generation of quick disconnect fittings. They were designed with improvements to mechanical reliability, and have greater durability across a wider temperature range. QDT quick disconnects are available with EPDM or Viton seals. An external color band identifies the o-ring material: silver is EPDM, black is Viton. (EPDM is recommended for Koolance liquids.)
Aug 13, 2021Inventory Delays
Due to global freight issues, we are experiencing significant delays in receiving some products. The availability dates shown on our website may be adjusted repeatedly based on the latest information.
Jun 21, 2021ALR-4500 CE Certification
Koolance's 900W recirculating liquid chiller is now available in a 220VAC (50-60Hz) version. This model is CE certified and is supplied with a CEE 7/7 "Type F" power cable.
Jul 10, 2020Shipments Are Resuming
As Koolance U.S. has been designated an essential business, we are resuming order processing again. Shipments from our U.S. location may incur a brief delay while we implement safety measures for COVID-19. Customer pickup is not available at the present time.
For all inquiries, please contact us via email, as our phone system is not currently staffed.
For all inquiries, please contact us via email, as our phone system is not currently staffed.
Jul 10, 2020Order Processing Delay
We are currently unable to ship orders from WA State through April 9th due to a government-mandated shutdown for COVID-19. Orders shipping from Koolance Korea, manufacturing, and development are unaffected during this period.
We will continue to answer email. Backorders can still be placed through our website, which will be shipped once restrictions are lifted. (Payment is required for backorders later when they are being prepared.)
We will continue to answer email. Backorders can still be placed through our website, which will be shipped once restrictions are lifted. (Payment is required for backorders later when they are being prepared.)
Dec 23, 2019New ALR-4500 Cooling Systems Available
ALR-4500 is Koolance's highest performance ambient liquid cooling series to date, with 4300W (ALR-4500A) and 4600W (ALR-4500C) of heat dissipation. They can be operated in vertical, horizontal, and rack mountable orientations, and each features built-in software control, flow rate reporting, and coolant level sensing.
Oct 14, 2019ERM-3K3UC Inventory Delay
The ERM-3K3UC cooling systems are expected back in stock in late October to mid-November.
Mar 14, 2019ALH-2000 Cooling & Heating System Available
ALH-2000 is an ambient liquid cooling system with heating capabilities to maintain a steady temperature for a non-constant heat load, or for a cold plate/sample which must stay near or above the ambient room temperature.
Feb 20, 2019Backorders Now Accepted
Out-of-stock products and quantities can now be backordered through Koolance.com. When the items are ready to ship, an email will be sent out to complete payment. Due to this, there are currently some limits placed on the total amount which can be backordered. A pre-deposit option is being developed to enable higher backordering limits.
Nov 28, 2018Koolance ISO 14001 Certification
In addition to ISO 9001, Koolance has now been certified for ISO 14001 (Environmental management system).
CTR-KSM100 is a liquid cooling system controller with both hardware and software interfaces. It incorporates a 2-line OLED display for user control and feedback, and a USB port for configuration and logging via the Koolance System Monitor application. Output power for 12V and 24V pumps is supported.
Apr 11, 2018CPU-400 Reviewed at Extreme Rigs
Extreme Rigs has reviewed Koolance's new CPU-400 water block:

The performance has increased and the CPU-400 holds the honor of the single best thermal result of all time... This is our new recommended block to buy for Intel setups.

Mar 26, 2018CPU-400 Now Available!
Koolance has released its best performance water block to date for Intel and AMD processors.
Sep 18, 2017High Pressure Quick Disconnects
Koolance has released new quick disconnects for high pressure applications. QD1H, QD2H, QD3H, and QD4H maintain their no-spill feature when disconnected at pressures up to 10kgf/cm2 (142psi). These series are not physically compatible with earlier versions.
It scored a top spot when paired with the overclocked Haswell-E processor, an impressive feat given [its] high-performance competitors.
Mar 31, 2017VLX-450 Chiller Subassembly Now Available
VLX-450 is a ready-to-integrate, inline, open frame chiller rated at 450W of cooling with a 0°C liquid-ambient delta. It is designed simply to be dropped into an existing cooling loop, which will move coolant through its stainless steel plate heat exchanger.
Mar 16, 2017New Modular ALX Cooling Systems Launched
Koolance's ALX series are powerful liquid cooling systems with expandable thermal capacities and software logging. ALX systems have up to twice the thermal capacity of previous Koolance ambient liquid cooling systems for the same heat exchanger size. As modular products, the radiator and pump units can be individually upgraded if requirements later change.
Feb 28, 2017CPU-390 Gets Support for AMD Socket AM4
Koolance CPU-390A and CPU-390CA water blocks now include support for AMD's socket AM4 (Ryzen, etc.). For existing owners of CPU-390, a separate upgrade kit is available to add compatibility.
Jan 11, 2017MD&M West Medical Expo Feb. 7-9



Stay Connected